NXP Simulink library for MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP Simulink library for MPC5777C

3,453 次查看
raman_nain
Contributor I

Hello,

I have been trying to use the CAN communication and ADC blocks with MBD_MPC574x_Config_Information block by selecting MPC5777C microprocessor but the CAN and ADC blocks shows the following error "The selected MCU has no support in MBDT for this peripheral".

Could you please let me know when the supporting blocks in the Simulink library for MPC5777C would be ready to use because I can't use them right now. Attached is the image shown below.

With best

Raman Nain

标签 (1)
3 回复数

3,265 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi raman.nain@aikar.io‌,

The peripherals support for MPC5777C in the version 3.1.0 is limited to UART and GPI/O.

Please refer to https://community.nxp.com/docs/DOC-345217 second bullet for explanation.

The MPC5777C was added initially for SIL/PIL and AUTOSAR SW-C Enablement. In mid April 2020 we are going to release version 3.2.0 which will incorporate the support for ADC/CAN and other peripherals.

Best regards,
Daniel

3,266 次查看
tjs
Contributor I

Hi Daniel-  any update ETA on the 3.2.0 release for  5777C support?

0 项奖励
回复

3,266 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Thomas, 

The MBDT for MPC57xx version 3.2.0 is scheduled for release next week on April 14th. It will have both peripherals discussed above + much more. 

Best regards,

Daniel

0 项奖励
回复