NXP Model-Based Design Toolbox for S32K1xx – version 4.1.0 import S32DS.2018r1 Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP Model-Based Design Toolbox for S32K1xx – version 4.1.0 import S32DS.2018r1 Error

1,262 次查看
297364116
Contributor I

Glad to welcome NXP Update 4.1 MBD Development Toolkit。There are many problems in use.

Configuration environment:

1.computer system:win10  64bit Professional 

2.Visual Studio 2017 Professional 

3.S32 Design Studio for ARM Version 2018.R1

4.Matlab 2018b 

5.Model-Based Design Toolbox for S32K1xx – version 4.1.0

Problem Description:As an example, no error message occurred when the code was generated.When imported into S32DS according to the configuration file XML, compiled and sent to the following error.Two compilation methods have been tried and error prompts appear.For details, please see the picture below.

pastedImage_1.png

pastedImage_2.pngpastedImage_3.png

pastedImage_4.png

pastedImage_5.png

pastedImage_6.png

pastedImage_7.png

标签 (2)
标记 (1)
0 项奖励
回复
0 回复数