Multiple PIL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple PIL

888件の閲覧回数
Jáuregui
Contributor I

Hi, I'm trying to run multiple PIL in a single Simulink project but it looks like multiple model blocks in PIL mode can't be used, the next error occurs when I try to run the project.

Juregui_0-1717455426481.pngJuregui_0-1717455426481.png

My setup:

Matlab version: 2017b

MBD version: NXP_MBDToolbox_S32K1xx_4.3.0

Simulink Model:

Juregui_1-1717455909460.pngJuregui_1-1717455909460.png

Both models are the gpio_s32k144 from the examples folder just with different names.

Juregui_2-1717456441656.pngJuregui_2-1717456441656.png

And I have two S32k144 connected to the computer through USB ports.
I want to know if it is possible or is there any other way to have two or more microcontrollers in a single simulation running independently.

S32K144EVB 

0 件の賞賛
返信
0 返答(返信)