More granular control of SPI timing on S32K1xx?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

More granular control of SPI timing on S32K1xx?

Jump to solution
1,117 Views
ranulf
Contributor IV

Are there any functions that provide more granular control of SPI timing than is available in the MBDT S32K1xx SPI config block?

0 Kudos
Reply
1 Solution
1,043 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

The S32K1 toolbox is based on SDK. You can go and check the files included in 'S32_Platform_SDK/platform/drivers/src/lpspi'.

Also, can you provide more information about what SPI timing you want to control?

Best regards,

Bancila Sorin

View solution in original post

0 Kudos
Reply
1 Reply
1,044 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

The S32K1 toolbox is based on SDK. You can go and check the files included in 'S32_Platform_SDK/platform/drivers/src/lpspi'.

Also, can you provide more information about what SPI timing you want to control?

Best regards,

Bancila Sorin

0 Kudos
Reply