Model-Based Design Toolbox for S32K3xx 1.5.0 Deploy Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Model-Based Design Toolbox for S32K3xx 1.5.0 Deploy Issue

963件の閲覧回数
Wei_H
Contributor III

Hi,

I have updated MBDT S32k3xx toolbox from 1.4 to 1.5 . After the update, deployment to the chip still go through the downloading process, however, the chip does not response. Let me know if there is an issue with setting in the configure tool or other problem that I have not resolve, thanks!

I have used the shared project from the community, it works great in 1.4 but encounter issue when updated to 1.5. The file is called Article 4 - MR-CANHUBK344_CAN.zip, which you can find in the link below.

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

タグ(3)
0 件の賞賛
返信
0 返答(返信)