Model Based Design Toolbox for S32K14x Automotive MCU rev2.0 Free cost?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Model Based Design Toolbox for S32K14x Automotive MCU rev2.0 Free cost?

1,988件の閲覧回数
hayaoki7
Contributor IV
0 件の賞賛
返信
2 返答(返信)

1,553件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi hayaoki7‌,

Indeed, all the Model-Based Design Toolboxes from NXP are now cost free. You can use it for free with no fee charge.

The entire suite & ecosystem (IDE for debugging, GCC toolchain, bootloaders) is provided for free - all you need to do is to have an NXP account to download the licences - also free of charge.

You need to have a Matlab environment with Embedded Coder toolbox in order to be able to generate the C code automatically. That is a cost you have to consider but from our point of view we assume you have already such environment.

Hope this helps!

Daniel

0 件の賞賛
返信

1,553件の閲覧回数
hayaoki7
Contributor IV

How Nice

Thank you

0 件の賞賛
返信