Many analog signal readings from the same EQADC module on the MPC5777C?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Many analog signal readings from the same EQADC module on the MPC5777C?

917件の閲覧回数
ranulf
Contributor IV

It would be helpful to see examples ADC readings made of 3 or more analog signals, preferably from the same EQADC module (either 0 or 1). Apparently the EQADC blocks have the ability to read from more than 2 analog signals, but neither the examples nor the documentation show how to do this. Both of the examples cover cases where only 2 analog signals are read.

How many analog signals can be read by each EQADC module and how many analog signals can be read by the two modules together? It would also be nice to see examples that demonstrate reading a large number of analog channels involving both modules.

0 件の賞賛
返信
1 返信

884件の閲覧回数
ranulf
Contributor IV

The MPC5777C is already supported. See Model-Based Design Toolbox for MPC57xx version 3.2.0

0 件の賞賛
返信