MSCAN communication for SKEAZ64MLH4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSCAN communication for SKEAZ64MLH4

3,469 Views
ekta_rathod
Contributor II

Hello,

I am trying to transmit the data over CAN bus for nxp controller (SKEAZ64MLH4) using Processor Expert auto-generated code in 'Codewarrior'. CAN lines are connected to the 'PEAK' CAN adapter and observing the output on an open source software 'BUSMASTER'. But output terminal is continuously giving bus error messages.

Also Interrupt for TX is not getting generated as it is not coming in TX ISR. I am unable to figure out the problem with the CAN transmission.

Code has been attached here. Please help me out to resolve this issue.

Regards,

Ekta Rathod

1 Reply

3,419 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected] ,

Unfortunately we only handle question regarding MATLAB/Simulink and our toolboxes on this community. I suggest you post your question on the Kinetis Microcontrollers community.

Kind regards,

Razvan.