MPC5744P for UART and I2C Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P for UART and I2C Interface

ソリューションへジャンプ
3,262件の閲覧回数
toddchou
Contributor I

Dear Sir 

I am Todd and use MPC5744 for a project . In datasheet , this MCU can program UART interface that using FlexLIN port . However , it did not write some I2C interface . I am not sure , can we program I2C interface that same using FlexLIN , FlexRay or which one can support I2C interface ? 

Looking forward for your feedback. 

Thank you and have a good day.

Todd

0 件の賞賛
返信
1 解決策
3,030件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

MPC5744P does not have any I2C hardware unfortunately; I'm not sure if you are developing a project using our Simulink toolbox, but if you do you will not find support for I2C as there are no hardware instances available. If you need to have I2C, you can use the SDK for MPC5744P - there you have software support for I2C, this meaning bit-banging of the protocol done by the CPU.

Hope this helps,

Razvan.

元の投稿で解決策を見る

2 返答(返信)
3,031件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

MPC5744P does not have any I2C hardware unfortunately; I'm not sure if you are developing a project using our Simulink toolbox, but if you do you will not find support for I2C as there are no hardware instances available. If you need to have I2C, you can use the SDK for MPC5744P - there you have software support for I2C, this meaning bit-banging of the protocol done by the CPU.

Hope this helps,

Razvan.

3,030件の閲覧回数
toddchou
Contributor I

Hello Razvan 

Thanks for your explanation. 

Have a good day 

Todd

0 件の賞賛
返信