MPC5744P MBD toolbox - Reset input for integrator block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P MBD toolbox - Reset input for integrator block

1,882 Views
ext-rafael_barb
Contributor III

Hi,

I can see in the model based design toolbox for MPC5744P in Simulink the integrator blocks without the reset input option.

Can you make an update to include the integrator blocks with the reset input?

Regards, Rafael

0 Kudos
Reply
1 Reply

1,793 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi [email protected]‌,

Have you tried to use the standard Simulink Discrete PID Controller ?

That block can be configured exactly as you have suggested - integrator with reset option.

pastedImage_1.png

To achieve this you have to:

1. select the Controller type as: I

pastedImage_3.png

2. select the appropriate integrator method

 pastedImage_4.png

3. enable the External reset option

pastedImage_7.png

Can you check on your side if this approach will address your use-case. If not, then we can add a feature request to add the capability on the AMMCLIB block to do this as well.

Thank you!

Daniel 

0 Kudos
Reply