MPC5744P DSPI example,A vital problem occurs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P DSPI example,A vital problem occurs.

1,831件の閲覧回数
秦祥林秦
Contributor I

When I use the MPC5744P DSPI examples, I find a problem.DSPI initialization process in the skip DISAB_IRQ (), directly into the DSPI_init.However, when the shield DSPI_init, the program has returned to normal.The initial value of the DSPI is not passed, and the default value becomes all 0.

0 件の賞賛
返信
1 返信

1,683件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

This community is about issues encountered with the Model-Based Design Toolboxes. As far as i can see from your attachment you are using stand-alone examples for MPC5744P.

Since you are not using Matlab/Simulink to generate the code automatically for DSPI on MPC5744, my suggestion to you is to ask this on a different community: MPC5xxx or the place you have took the examples from.

Thank you!

Daniel 

0 件の賞賛
返信