MPC5744P Code does not run

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P Code does not run

1,800 Views
279814392
Contributor II

Dear Daniel

Thank you for your reply,I'm using 'Model Based Design ToolBox for MPC574xP', I want to read the register(CNTR) of etimer0,the address is 0xFBC2000C,and I add 'DataMemRead' module to read the CNTR value,then I debug in  freemaster,but the code can not run.

pastedImage_1.png

pastedImage_2.png

this is running status,all variable can not change,my simulink module will sent you by e-mail of [email protected].please help me!

Yuyuan Wang.

0 Kudos
Reply
1 Reply

1,629 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Yuyuan, 

Have you applied all the patches for MPC5744P toolbox ? The patches can be found here: HotFix: MBD Toolbox rev2.0.0 for MPC5744P (Panther) 

I think your problem is related with patch number #3 https://community.nxp.com/thread/451804#comment-916493 

If you use the S32 Design Studio for PA 1.2 or S32 Design Studio for PA 2017.R1 GCC compilers then you need to apply this patch or otherwise the program will not exit the startup sequence.

Hope this helps!

Daniel

0 Kudos
Reply