MPC5643L download error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5643L download error

1,970 Views
hongjinzeng
Contributor IV

Hi everyone,

  While I build the DigitalIO_block_demo,an error occur.

pastedImage_3.png

### Generating code into build folder: D:\matlab_work\DigitalIO_block_demo_rappid_rtw ### Generated code for 'DigitalIO_block_demo' is up to date because no structural, parameter or code replacement library changes were found.

### Evaluating PostCodeGenCommand specified in the model

### Processing Template Makefile: C:\MCToolbox\rappid564xl\rappid564xl\rappid_564xl_cw_2013.tmf

### DigitalIO_block_demo.mk which is generated from C:\MCToolbox\rappid564xl\rappid564xl\rappid_564xl_cw_2013.tmf is up to date

### Building DigitalIO_block_demo: .\DigitalIO_block_demo.bat

D:\matlab_work\DigitalIO_block_demo_rappid_rtw>set MATLAB=C:\Program Files\MATLAB\R2014a

D:\matlab_work\DigitalIO_block_demo_rappid_rtw>"C:\Program Files\MATLAB\R2014a\bin\win32\gmake" -f DigitalIO_block_demo.mk GENERATE_ERT_S_FUNCTION=0 INCLUDE_MDL_TERMINATE_FCN=1 COMBINE_OUTPUT_UPDATE_FCNS=1 MULTI_INSTANCE_CODE=0 INTEGER_CODE=0 clean

RELATIVE_PATH_TO_ANCHOR is ..

==== Removing object files from build directory ====

Copying necessary files to build directory...

Compiler details : "C:/Freescale/CW MCU v10.7/MCU/PA_Tools/Command_Line_Tools/mwcceppc" -vle -DVLE_IS_ON -gdwarf-2 -fp spfp_only -spe_vector -char unsigned -proc Zen -gccincludes -nostdinc -nosyspath -ansi off -opt all -bool on -Cpp_exceptions off -prefix "C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/EWL_C/include/lib_ewl.prefix" -I. -I.. -I"C:\Program Files\MATLAB\R2014a"\simulink\include -I"C:\Program Files\MATLAB\R2014a"\extern\include -I"C:\Program Files\MATLAB\R2014a"\rtw\c\src -I"C:\Program Files\MATLAB\R2014a"\rtw\c\libsrc -I"C:\Program Files\MATLAB\R2014a"\rtw\c\src\ext_mode\common -I"C:\Program Files\MATLAB\R2014a"\rtw\c\src\ext_mode\tcpip -I"C:\Program Files\MATLAB\R2014a"\rtw\c\src\ext_mode\serial -I"C:\Program Files\MATLAB\R2014a"\rtw\c\src\ext_mode\custom -I"C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/EWL_Runtime/Runtime_PA/Include" -I"C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/EWL_Runtime/Runtime_PA/Source" -I"C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/lib" -I"C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/EWL_C/include" -I"C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/EWL_C++/include" -ID:\matlab_work\DigitalIO_block_demo_rappid_rtw -ID:\matlab_work -DUSE_RTMODEL -DMODEL=DigitalIO_block_demo -DREAL_T=float -DRT -DNUMST=1 -DTID01EQ=0 -DNCSTATES=0 -DMT=0 -DHAVESTDIO -c Assembler details : "C:/Freescale/CW MCU v10.7/MCU/PA_Tools/Command_Line_Tools/mwasmeppc" -vle -DVLE_IS_ON -proc Zen -list -gccincludes -nostdinc -c

Building assembly file crt0.o...

Building assembly file sw_handlers.o...

Building assembly file excep_handler.o...

Building file DigitalIO_block_demo.o...

Building file gpio_564xl_library.o...

Building file gt_pf.o...

Building file intc_init.o...

Building file intc_sw_vectable.o...

Building file pit_ch1_isr.o...

Building file pit_ch2_isr.o...

Building file pit_ch3_isr.o...

Building file pit_timer_564xl_library.o...

Building file profile_buffer.o...

Building file rappid_main.o...

Building file rappid_utils.o...

Building file siu_init.o...

Building file sys_init.o...

Building file sysclk_init.o...

==== Creating DigitalIO_block_demo.out from obj files ====

"C:/Freescale/CW MCU v10.7/MCU/PA_Tools/Command_Line_Tools/mwldeppc" crt0.o sw_handlers.o excep_handler.o DigitalIO_block_demo.o gpio_564xl_library.o gt_pf.o intc_init.o intc_sw_vectable.o pit_ch1_isr.o pit_ch2_isr.o pit_ch3_isr.o pit_timer_564xl_library.o profile_buffer.o rappid_main.o rappid_utils.o siu_init.o sys_init.o sysclk_init.o -o DigitalIO_block_demo.elf -gdwarf-2 -fp spfp_only -char unsigned -proc Zen -m _start -nostdlib -srec -lcf MPC564xLRAM.lcf "MCLIB_MPC564xL.PPCEABI.V.UC.a" "C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/lib/libc_E200z446_VLE_SPFP_Only.a" "C:/Freescale/CW MCU v10.7/MCU/PA_Support/ewl/lib/librt_E200z446_VLE_SPFP_Only.a" -Map DigitalIO_block_demo.map

Created executable: DigitalIO_block_demo.elf

Building target all

*** Created executable: DigitalIO_block_demo.elf

### Successful completion of build procedure for model: DigitalIO_block_demo

D:\matlab_work>"C:\MCToolbox\rappid564xl\tools\BootLoader\RAppID_BL.exe" "C:\MCToolbox\rappid564xl\tools\BootLoader\\" "D:\matlab_work\DigitalIO_block_demo_rappid_rtw\DigitalIO_block_demo.rbl"

An unhandled exception occurred: System.ArgumentOutOfRangeException: Index was out of range. Must be non-negative and less than the size of the collection.

Parameter name: startIndex

In System.ParseNumbers.StringToInt(String s, Int32 radix, Int32 flags, Int32* currPos)

In System.Convert.ToInt32(String value, Int32 fromBase)

In RAppID_BL.GUI_Driver.GetCommChannel()

In RAppID_BL.GUI_Driver.StartBTL(String homeDir, Boolean showProgBar)

In RAppID_BL.MainProgram.Main(String[] args)

Build process completed successfully

0 Kudos
Reply
1 Reply

1,658 Views
raduivan
NXP Employee
NXP Employee

Hi Hongjin,

   Please check that you have some device connected to COM1 or other COM, if you don't have any device connected please remove the download option. This is issue is already logged  and in process to be fixed by the Bootloader team.

Best regards,

Radu