MCToolBox example project "adc_pdb_trigger_s32k14.mdl"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCToolBox example project "adc_pdb_trigger_s32k14.mdl"

3,093 Views
fengwang
Contributor I

Hi Radu,

     I use MCToolBox example project "adc_pdb_trigger_s32k14.mdl" , occur this error . Could you help me kill this error ?

pastedImage_1.png

 Thanks !

Regards,

     Feng

0 Kudos
Reply
3 Replies

2,777 Views
raduivan
NXP Employee
NXP Employee

Hi Feng,

   Please delete and remake the link between ADC block and output port. From the screenshot you attached, the error occurs because those two blocks are not connected.

Best regards,

Radu

0 Kudos
Reply

2,777 Views
fengwang
Contributor I

Hi Radu,

     Thank you for me to solve error  again and again.

     I installed the "Motor Control Toolbox" again , i building the project in the simulink ,occur this error  :

pastedImage_1.png

i can't understand the "setting  up the target compilers" like this ; How can i  do it follow this .

pastedImage_2.png

 Many many thanks !

Best regards,

Feng

0 Kudos
Reply

2,777 Views
raduivan
NXP Employee
NXP Employee

Hi Feng,

   First you need to install the compiler you intend to use and after you need to set an Environment variable which will point to the installation folder. Let me know if you need more information.

Best regards,

Radu

0 Kudos
Reply