MC9S12VML128 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12VML128 MCU

1,434 Views
zhuaoci
Contributor II

The compressed file in the attachment is the generated code. The compiler that I use is CW for MCU v10.6,And the chip is MC9S12VML128 MCU. But I can't find the project files, I don't know how to import them into the compiler, generate the project files, and then download them into the chip.

Tags (1)
0 Kudos
Reply
2 Replies

1,192 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi zhuaoci‌,

You can simply configure the Matlab Toolbox for download the code directly to the target. No need to import it in CW for MCU to recompile and download.

Please have a look here: https://community.nxp.com/community/training/ftf-2015-training-presentations/projects/hands-on-motor... starting with slide #40

Hope it helps!

Daniel

0 Kudos
Reply

1,192 Views
zhuaoci
Contributor II

The following figure showsBut I can't find the Simulink model below.QQ截图20171024200736.pngQQ截图20171024200811.png

0 Kudos
Reply