MC33771C PCB does not initialize through MBDT projects. Does through GUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33771C PCB does not initialize through MBDT projects. Does through GUI

855 Views
Poley
Contributor V

Hi all,

 

I have a custom MC33771C PCB that is 14S but I have it setup to read 11S througb the connector by connecting cell 4 to 5, 6 and 7 as well. I have use a few different custom MC33771C's previously and not had any issues. However, this board is acting very weird. Whenever I try and load MBDT code onto it the device switched off straight away (Shown by VCOM light) and reports a Status of "3" from BCC_INIT. I am trying to use a single CMU with TPL.

What is weird is that the MC33771C GUI when connected to the S32K144EVB through the MC33664 breakout board to my custom MC33771C works absolutely fine. I am just confused about what could be causing the MBDT examples from not working compared to the GUI?

The only other this I noticed was that the voltage values seem to take a second or so to get up to the correct voltage measurement values(Video attached), is this normal?

Thanks in advance!

0 Kudos
Reply
0 Replies