MBDToolbox for S12ZVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDToolbox for S12ZVM

65,199 Views
almin_svraka
Contributor I

Hello,

For some time I have been trying to add MBDToolbox for S12 ZVM to Matlab unsuccessfully.
I was able to add MBDToolbox for S12 ZVC to Matlab; however, I need to have a toolbox for S12ZVM in Simulink.
In addition, there is a setup file for S12ZVC toolbox, and it worked fine, but no setup file for S12ZVM.
The script (m file) that comes with NXP_Support_Package_S12ZVMx_20200907 does nothing.
Basically, it runs and at the end it says that the toolbox was added, but it is not added- No MBDToolbox in Simulink.

I tried with Matlab 2020b and Matlab 2020a and it doesn't work for neither.

Please advise !

Almin

Tags (1)
0 Kudos
Reply
22 Replies

7,076 Views
almin_svraka
Contributor I

Hello,

I have the license for MBDToolbox.

I provided some information and I generated the license on site a few weeks ago.

So, I do not have a license error.

Best Regards,

Almin

 

0 Kudos
Reply

1,115 Views
almin_svraka
Contributor I

Hello,

I thank you for your quick reply.

As I said Matlab Ad-On Manager see S12ZVM toolbox.

I think I showed you the returns from running ver command.

>> ver
-----------------------------------------------------------------------------------------------------
MATLAB Version: 9.8.0.1451342 (R2020a) Update 5
MATLAB License Number: DEMO
Operating System: Microsoft Windows 10 Pro Version 10.0 (Build 19041)
Java Version: Java 1.8.0_202-b08 with Oracle Corporation Java HotSpot(TM) 64-Bit Server VM mixed mode
-----------------------------------------------------------------------------------------------------
MATLAB Version 9.8 (R2020a)
Simulink Version 10.1 (R2020a)
Embedded Coder Version 7.4 (R2020a)
IEC Certification Kit Version 3.15 (R2020a)
MATLAB Coder Version 5.0 (R2020a)
Model-Based Design Toolbox for S12ZVMx Series Version 1.4.0 (R2015a-R2020a)
Simulink Coder Version 9.3 (R2020a)
Stateflow Version 10.2 (R2020a)
>>

I have two Matlab versions: 2020a and 2020b which is the latest release.

Matlab 2020b is licensed and it works fine; however, I was told that this version doesn't support nxp S12ZVM toolboox yet, but the previous version does support. So, I downloaded Matlab 2020a (download link sent by Mathworks support personnel), and I have been trying to add S12ZVM toolbox for some time.

I ran the the example, adc_s12zvm, from the directory where it is and doesn't build - error is generated (missing files).

Please Advise

Almin

0 Kudos
Reply