MBDT version for S32K396-LQFP-DC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT version for S32K396-LQFP-DC

Jump to solution
1,662 Views
Silvano
Contributor I
I would like to ask you if there is a Model-Based Design Toolbox for the LQFP version of the S32K396 MCU ?
 
On the NxP website, the last version (1.4.0) supports only the BGA version for the S32K396 MCU and integrates RTD v.3.0  however the LQFP version requires RTD v.4.0.
 
 
Thank you for your help,
0 Kudos
Reply
1 Solution
1,628 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hello @Silvano 

Indeed, the current MBDT for S32K3 version 1.4.0 integrates the RTD 3.0.0, and provides support for the S32K396 BGA289 MCU. The future MBDT for S32K3 release, version 1.5.0, will integrate RTD 4.0.0. For being able to conduct an analysis with respect to adding support for S32K396 LQFP176, it would be useful for us to know what is the hardware that is being targeted for this design.

To provide some context, as part of offering support for a processor, or a derivative, MBDT delivers default configuration projects (EB Tresos and S32 Configuration Tools) targeting specific MCUs. The default projects contain comprehensive configurations of Pins, Clocks and Peripherals, according to the NXP evaluation boards that were available for development and testing. For example, the S32K396 BGA289 configuration, and the S32K396 example models delivered inside our toolbox, are addressing the hardware resources on the S32K396-BGA-DC evaluation board.

In case of a custom hardware design, specific on-board configurations can be created starting from the default ones (the default ones we enable are targeting only NXP hardware). Yet, we offer the possibility of customizing these configurations and use MBDT with customer specific designs - there are some steps that could be performed for updating, for example, the S32K396 BGA289 configuration project to target S32K396 LQFP176. For this, we could provide the necessary guidance on how to modify the existing settings to target specific Peripherals, Pins, and other on-board configuration settings.

Given this context, could you please let us know more details on the use case and setup that you would like to achieve, so that we could provide support in accordance to your needs?

Thank you,
Irina

View solution in original post

0 Kudos
Reply
1 Reply
1,629 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hello @Silvano 

Indeed, the current MBDT for S32K3 version 1.4.0 integrates the RTD 3.0.0, and provides support for the S32K396 BGA289 MCU. The future MBDT for S32K3 release, version 1.5.0, will integrate RTD 4.0.0. For being able to conduct an analysis with respect to adding support for S32K396 LQFP176, it would be useful for us to know what is the hardware that is being targeted for this design.

To provide some context, as part of offering support for a processor, or a derivative, MBDT delivers default configuration projects (EB Tresos and S32 Configuration Tools) targeting specific MCUs. The default projects contain comprehensive configurations of Pins, Clocks and Peripherals, according to the NXP evaluation boards that were available for development and testing. For example, the S32K396 BGA289 configuration, and the S32K396 example models delivered inside our toolbox, are addressing the hardware resources on the S32K396-BGA-DC evaluation board.

In case of a custom hardware design, specific on-board configurations can be created starting from the default ones (the default ones we enable are targeting only NXP hardware). Yet, we offer the possibility of customizing these configurations and use MBDT with customer specific designs - there are some steps that could be performed for updating, for example, the S32K396 BGA289 configuration project to target S32K396 LQFP176. For this, we could provide the necessary guidance on how to modify the existing settings to target specific Peripherals, Pins, and other on-board configuration settings.

Given this context, could you please let us know more details on the use case and setup that you would like to achieve, so that we could provide support in accordance to your needs?

Thank you,
Irina

0 Kudos
Reply