MBDT support for MC33774

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT support for MC33774

1,377件の閲覧回数
Yusuf
Contributor I

Hello,

I am using MC33774 bcc for a bms project with S32K344 bmu. It is already supported by S32 configuration tool and the drivers can be generated but it is not supported by MBDT simulink libraries. What is the easiest way to integrate Bcc_774a drivers into MBDT environment as it is already for the existing ones like MC33775? or as an another version of the same question: What is the general method for building driver blocks for any ordinary IC in MBDT environment using S32K3 processors? Could you please share any documentation, tutorials etc.?

Thanks

0 件の賞賛
返信
1 返信

1,194件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @Yusuf ,

This week we have released the Model-Based Design Toolbox for BMS version 1.1.0, which adds support for the MC33774 in Simulink. The toolbox provides ready-to-run examples for the possible use cases of MCU/PHY/CMU combinations together with a guideline of the key components you need to take care about:

  • S32K344 + MC33665 + MC33774A - k344bmu_774a_read_s32ct.mdl or EB tresos Studio
  • S32K358 + MC33665 + MC33774A - k358bmu_774a_read_s32ct.mdl or EB tresos Studio
  • S32K344 + MC33664 + MC33774A - s32k344_664_774_s32ct.mdl

Please let us know if there are any questions!

Regards,

Marius

0 件の賞賛
返信