MBDT license issue: S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT license issue: S32K144

5,810件の閲覧回数
Nikhiladheesh
Contributor II

After integrating with Simulink environment, unable to build project.

Please find license file used and also error message.

 

 

0 件の賞賛
返信
5 返答(返信)

5,685件の閲覧回数
mv3234
Contributor II

As per the suggestion, i downloaded the s32k144 package and convert it to the .mltbx package but it is not working

0 件の賞賛
返信

5,792件の閲覧回数
Nikhiladheesh
Contributor II

Hi Nathan,

 

Thanks for your response, i have generated free license. But i cannot use it with Simulink as it is throwing me an error.

Can you please let me know what can i do? I also referred previous thread to understand why the license issue is popping up. But it did not help me.

0 件の賞賛
返信

5,767件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @Nikhiladheesh,

My guess is that the license is not installed in the right location, or the name is not right. To investigate, please run the following command inside the MATLAB's Command Window:

winopen(fullfile(mbd_find_s32k_root, 'lic'))

This will open a window in which there should be the license file, typed exactly like this: "license.dat" or "license.lic".

mariuslucianand_0-1650959705378.png

Regards,

Marius

 

5,763件の閲覧回数
Nikhiladheesh
Contributor II

license.dat format worked now, license.lic was not recognised.

5,795件の閲覧回数
Nathan69
Contributor I

You can generate the free license and access training & support on NXP Model Based Design Toolbox Community.

0 件の賞賛
返信