MBDT import library error in MCSPTE1AK144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MBDT import library error in MCSPTE1AK144

跳至解决方案
6,365 次查看
RajG
Contributor III

Hello @Daniel_Popa  and all members, I am using MCSPTE1AK144 motor control toolkit. I have installed MBDT v 4.2.0 with MATLAB R2018b, Simulink 9.2 but I am facing issues when I try to load the examples downloaded from Module 5 V/F Scalar Control of " 3-Phase PMSM Control Workshop with NXP's Model-Based Design Toolbox ". (I am downloading M5_2018.R1.zip file how ever I also tried with M5.zip and still show similar error)

I will attach the screenshots so that it will be clear. I have also written my query in image itself. 

errors_simulink_0.png shows the warning when I open the file provided at bottom.

errors_simulink_1.png shows the two type of issues which I am facing.

errors_simulink_2.png shows that I can replace some type of block but cannot replace other types.

 

I have also posted this question of Module 5 page of workshop. Help me to understand the issues.

Thanks and Regards,

RajG.

标签 (1)
0 项奖励
回复
1 解答
6,347 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @RajG ,

The models in the course are released in an older version of MBDT toolbox. The logic is the same but some blocks have to be manually replaced with the ones from the latest toolbox, like the new AMMCLIB blocks.

You can find the final models already in the toolbox.

mariuslucianand_0-1614591476547.png

Hope this helps,

Marius

在原帖中查看解决方案

0 项奖励
回复
3 回复数
6,348 次查看
RajG
Contributor III

I suppose there was some issue when I uploaded the images, so here I am again re-uploading them.

Help me I am still stuck..

Thanks and Regards,

RajG.

0 项奖励
回复
6,348 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @RajG ,

The models in the course are released in an older version of MBDT toolbox. The logic is the same but some blocks have to be manually replaced with the ones from the latest toolbox, like the new AMMCLIB blocks.

You can find the final models already in the toolbox.

mariuslucianand_0-1614591476547.png

Hope this helps,

Marius

0 项奖励
回复
6,330 次查看
RajG
Contributor III

thanks for the reply, I am trying to load and run V/F open loop method and in the Hardware setup it says to plug connector J9,J10 and J11 on position 2-3 ( will attach screenshot of the same below). My doubt is that V/F doesn't require any of the feedback then how the model works correctly?

0 项奖励
回复