MBDT for i.MX RT 105x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT for i.MX RT 105x

ソリューションへジャンプ
1,403件の閲覧回数
gianpiero_lenta
Contributor I

Is the MBDT supported by the RT105x microprocessor?
From the document "NXP Model-Based Design Toolbox (MBDT) Fact Sheet" it would appear that the micro 105x is not supported.
Who can answer me?

What I don't quite understand is this:
the 106x and 105x share cores, peripheral architecture, and differ only in the amount of internal RAM. Correct? Then why is MBDT not supported?

Thank you

0 件の賞賛
返信
1 解決策
1,374件の閲覧回数
stefancinipeanu
NXP Employee
NXP Employee

Hello @gianpiero_lenta 

Currently, the NXP`s MBD Toolbox for IMXRT1xxx platform does not support IMXRT105x and we do not have any plans to add it in the near future, but we are going to analyze this option.

Regards,

Stefan.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,375件の閲覧回数
stefancinipeanu
NXP Employee
NXP Employee

Hello @gianpiero_lenta 

Currently, the NXP`s MBD Toolbox for IMXRT1xxx platform does not support IMXRT105x and we do not have any plans to add it in the near future, but we are going to analyze this option.

Regards,

Stefan.

0 件の賞賛
返信