MBDT for S32k344 Dual Core Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT for S32k344 Dual Core Configuration

Jump to solution
2,530 Views
Wei_H
Contributor III

Hello, for the S32k344 board, is there any option to configure it on Simulink to use each core separately in the MBDT on Simulink?

Tags (2)
0 Kudos
Reply
1 Solution
1,677 Views
dragostoma
NXP Employee
NXP Employee

Hi,

We are currently assessing the addition of multicore support for the S32K3 toolbox in the next release planned for the end of the year. Unfortunately, we do not have any documents prepared that could help you integrated the multicore for S32K3 in Simulink.

We will follow up with additional details as soon as possible.

 

Best regards,

Dragos

View solution in original post

5 Replies
2,510 Views
kodyw
Contributor III

Hi @dragostoma ,

We developed a product using S32K344 with NXP S32K3xx MBDT tools and encountered some performance issues with the single core (lockstep mode).  We are wondering if we can configure it as decoupled mode.  However, S32K3xx MBDT tools do not support it yet.  How can we request this multi-core support for S32K3xx MBDT tools? Thanks,

Kody

Tags (3)
0 Kudos
Reply
2,069 Views
dragostoma
NXP Employee
NXP Employee

Hi, @kodyw,

For an official request, you can submit a support ticket through the nxp.com website here or contact your NXP sales representative in your region.

 

Best regards,

Dragos

 

0 Kudos
Reply
1,975 Views
kodyw
Contributor III

@dragostoma ,

We created a support ticket last month but NXP David Tosenovjan redirect the support back to this community.  Do you have some documents or 3rd party company that can help on using multicore for the S32K3 MBDT within Simulink?    Maybe some Simulink pre-compile/post-compile scripts can make it work or that is not possible? 

Thank you,

Kody

0 Kudos
Reply
1,678 Views
dragostoma
NXP Employee
NXP Employee

Hi,

We are currently assessing the addition of multicore support for the S32K3 toolbox in the next release planned for the end of the year. Unfortunately, we do not have any documents prepared that could help you integrated the multicore for S32K3 in Simulink.

We will follow up with additional details as soon as possible.

 

Best regards,

Dragos

1,664 Views
kodyw
Contributor III

@dragostoma 

Thank you very much for the update!

We can't wait to see the next release for the multi-core support for S32K3.

Best regards,

Kody

0 Kudos
Reply