MBDT for S12ZVMBEVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT for S12ZVMBEVB

4,865 Views
m_benderradji
Contributor II

Hello,

From what I understand, the MBDT is compatible with the family of S12ZVMB MCUs.
I want to design an application using evaluation board S12ZVMBEVB (refer to the following link)

S12ZVMB Evaluation Board|NXP 
Could you please tell me where I can find examples (motor control or others).
For S12ZVMB Evaluation Board|NXP which library sould i use ? (refer please to the following) 1 or 2 or 3

pastedImage_2.png

Thanks in advance for your support

Best regards

0 Kudos
Reply
7 Replies

4,258 Views
Jeffries
Contributor I

Thank you so much to sharing this post.

0 Kudos
Reply

4,668 Views
m_benderradji
Contributor II

Hello,

In the NXP web page dedicated to the MBDT https://www.nxp.com/support/developer-resources/run-time-software/automotive-software-and-tools/mode... 

It is indicated that the toolbox support the S2ZVMB (refer to the following)

pastedImage_1.png

There is a contradiction, right?

0 Kudos
Reply

4,668 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

You are right - that should probably not be on the product web page.

Thank you for pointing it out!

Kind regards,

Razvan.

0 Kudos
Reply

4,668 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

S12 Toolbox supports the following parts (as stated in the release notes)

pastedImage_1.png

So the toolbox does not support S12ZVMB unfortunately (not tested on). I do not know what are the differences between them. If they are very similar, the toolbox could be ported.

Kind regards,

Razvan.

0 Kudos
Reply

4,330 Views
SUT
Contributor I
Can the toolbox support s12zvmb? I can see that s12zvmb is still available on the product web page
0 Kudos
Reply

4,319 Views
adriantudor
NXP Employee
NXP Employee

Hello @SUT ,

 

The answer given by Razvan is still up to date. Anyway, the S12ZVMBEVB development board was designed to drive DC two-phase motor using H-bridge, while the MBDT for S12ZVM has only BLDC/PMSM examples.

 

Best regards,

Adrian

0 Kudos
Reply

4,669 Views
m_benderradji
Contributor II

Hello NXP tram,

Any feedback please ?

Thanks in avance

0 Kudos
Reply