MBDT Support for GoldBox Peripherals (CAN, ENET etc)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT Support for GoldBox Peripherals (CAN, ENET etc)

1,666 Views
MattSoda
Contributor I

Hi,

We have a .GoldBox (S32G2). I have downloaded the HCP Toolbox (1.3.0) and there is only support for SIL/PIL, with only blocks being the Data Memory Read/Write. Is there any support for peripheral functions such as CAN, Ethernet,any other communication or system functions? Or is there any plan to implement this in the future?

Thanks
Matt

0 Kudos
Reply
1 Reply

1,590 Views
paulvlase
NXP Employee
NXP Employee

 Hello @MattSoda ,

 

The MBDT for HCP toolbox currently supports only MIL/SIL/PIL simulations. There is no support for peripheral functions, and right now there are no plans to implement it.

I would recommend you to open a support ticket on the nxp.com website to submit a request for this support.

 

Best regards,

Paul