MBDT: Can't update SPI message using StateFlow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT: Can't update SPI message using StateFlow

1,048件の閲覧回数
DN_at_Rix
Contributor I

I'm working with the MPC5744P and trying out Stateflow in addition to the required #MBDT software. I'm interfacing with an SPI module and trying a sequence of steps to confirm proper communication and that a register write did in fact complete. It looks really nice in stateflow, but I couldn't get the input/output data to take effect on the SPI message. When I built a if statement version it seems to be working. It's not as pretty though, so I really hope I'm just missing something. Attached are screenshots of my working and non-working versions of the same code.

top_level.png

^ Top level

 

working_SPI.png

^ Working SPI trigger

 

non_working_SPI.png

^ Non working SPI trigger 

タグ(3)
0 件の賞賛
返信
0 返答(返信)