MBD uses custom C code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBD uses custom C code

1,633 Views
m15871781742
Contributor II

Hello everyone:

      I am going to develop a Battery Manage System. I will use MPC5744P and MC33771C and I want to use the MBD method. I have download the MC33771C driver from the NXP website, I need to import the C code to the Simulink model.

      So, I made some attempts. The Hardware is the DEVKIT-MPC5744P, the C code is the hello world program in the S32DS library. when I build the model, I got some error message.

       I attached the program file. Hope someone can help me, thank you.

c_to_matlab.jpgmodel.jpgmodel2.jpgerror1.jpgerror1.jpgerror2.jpgerror3.jpg

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies