MBD for MPC5744P Code S32 Complier

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBD for MPC5744P Code S32 Complier

814件の閲覧回数
xingzhenlei
Contributor II

Problem 1: As shown in the figure below, why can't I see the source code for some functions? Is it because they are encapsulated in the "MPC574xP_AMMCLIB.a" file? Where can I find specific function comments and calling methods?

(#define ADC_INST_HAS_CWSELRn(inst,x) (ADC_INST_HAS_REG_4(inst,x)))

xingzhenlei_0-1725808668998.png

 

Problem 2: If they are indeed encapsulated in the aforementioned file and I cannot see the comments or calling methods, what materials should I use to write my own library files?

 

The source code and library files are attached.

タグ(1)
0 件の賞賛
返信
0 返答(返信)