MBD for MPC5744P Code S32 Complier

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MBD for MPC5744P Code S32 Complier

810 次查看
xingzhenlei
Contributor II

Problem 1: As shown in the figure below, why can't I see the source code for some functions? Is it because they are encapsulated in the "MPC574xP_AMMCLIB.a" file? Where can I find specific function comments and calling methods?

(#define ADC_INST_HAS_CWSELRn(inst,x) (ADC_INST_HAS_REG_4(inst,x)))

xingzhenlei_0-1725808668998.png

 

Problem 2: If they are indeed encapsulated in the aforementioned file and I cannot see the comments or calling methods, what materials should I use to write my own library files?

 

The source code and library files are attached.

标记 (1)
0 项奖励
回复
0 回复数