MBD Toolobox for S32K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBD Toolobox for S32K

ソリューションへジャンプ
6,416件の閲覧回数
alessandropinta
Contributor I

Does anyone know about error "Undefined function 'slsfnagctlr' for input arguments of type 'char'"?

I got it during code generation of every example of MBD Toolbox S32K, using Matlab2017b. Do you think that is a Matlab incompatibility issue?

Thanks in advance!

Original Attachment has been moved to: test_adc.slx.zip

1 解決策
5,951件の閲覧回数
alessandropinta
Contributor I

Hi dumitru-daniel.popa‌,

It's working now with toolbox v 3.0.0.

Thank you very much for your support!

Regards,

Alessandro

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,951件の閲覧回数
raghurajappa
Contributor IV

dumitru-daniel.popa‌ , We're facing a similar issue with the MCT Toolbox for the MPC564xL. It works with 2017a but not 2017b for similar reasons. Would there be a fix for this? If yes, when can I expect it? If no, can we have a workaround? 

0 件の賞賛
返信
5,951件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

We are currently working on a workaround to enable older toolboxes for running into the newer versions of the MATLAB 2017b and 2018a. Currently the fix is under testing on MPC564xL but we had some issues with the lack of HW to test on. 

Stay tuned - the fix will be soon available.

Thank you for your patience and for using the tools.

Best regards,
Daniel

0 件の賞賛
返信
5,951件の閲覧回数
raghurajappa
Contributor IV

thank you for your reply. I have tagged you in another question. Please help me with that. 

0 件の賞賛
返信
5,951件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi alessandropintabona‌,

I presume you are using the toolbox v2.0.0 right ? That does not have the support for 2017b release because the Matlab changed the API. It works only until 2017a.

But, yesterday we launched v.3.0.0 version that is fully supported in 2017b: https://community.nxp.com/docs/DOC-335555 

Perhaps you can upgrade to this one.

Best regards,
Daniel

5,952件の閲覧回数
alessandropinta
Contributor I

Hi dumitru-daniel.popa‌,

It's working now with toolbox v 3.0.0.

Thank you very much for your support!

Regards,

Alessandro

0 件の賞賛
返信