MBD Toolobox for S32K

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MBD Toolobox for S32K

跳至解决方案
6,419 次查看
alessandropinta
Contributor I

Does anyone know about error "Undefined function 'slsfnagctlr' for input arguments of type 'char'"?

I got it during code generation of every example of MBD Toolbox S32K, using Matlab2017b. Do you think that is a Matlab incompatibility issue?

Thanks in advance!

Original Attachment has been moved to: test_adc.slx.zip

1 解答
5,954 次查看
alessandropinta
Contributor I

Hi dumitru-daniel.popa‌,

It's working now with toolbox v 3.0.0.

Thank you very much for your support!

Regards,

Alessandro

在原帖中查看解决方案

0 项奖励
回复
5 回复数
5,954 次查看
raghurajappa
Contributor IV

dumitru-daniel.popa‌ , We're facing a similar issue with the MCT Toolbox for the MPC564xL. It works with 2017a but not 2017b for similar reasons. Would there be a fix for this? If yes, when can I expect it? If no, can we have a workaround? 

0 项奖励
回复
5,954 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

We are currently working on a workaround to enable older toolboxes for running into the newer versions of the MATLAB 2017b and 2018a. Currently the fix is under testing on MPC564xL but we had some issues with the lack of HW to test on. 

Stay tuned - the fix will be soon available.

Thank you for your patience and for using the tools.

Best regards,
Daniel

0 项奖励
回复
5,954 次查看
raghurajappa
Contributor IV

thank you for your reply. I have tagged you in another question. Please help me with that. 

0 项奖励
回复
5,954 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi alessandropintabona‌,

I presume you are using the toolbox v2.0.0 right ? That does not have the support for 2017b release because the Matlab changed the API. It works only until 2017a.

But, yesterday we launched v.3.0.0 version that is fully supported in 2017b: https://community.nxp.com/docs/DOC-335555 

Perhaps you can upgrade to this one.

Best regards,
Daniel

5,955 次查看
alessandropinta
Contributor I

Hi dumitru-daniel.popa‌,

It's working now with toolbox v 3.0.0.

Thank you very much for your support!

Regards,

Alessandro

0 项奖励
回复