JN-AN-1069 Serial Cable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN-AN-1069 Serial Cable

2,162 Views
trungosu
Contributor II

I tried to run this application on 2 JN5169-001-M00 modules. One uses as a Coordinator. Another uses as an End.
The LED0,1 flashing together and LED0 (Transmitter) always turn ON on both. So I think the connection is good.
However, I try to connect FTDI cable to both modules on UART0 with baud rate 115200.
I tried to send from one module "aaa" but never receive anything from another module.
I don't know if I have to follow any message format.

Thank you very much

0 Kudos
Reply
2 Replies

1,992 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi trungosu‌

I'm afraid i do not fully understand the background here? Is the application you are trying to run build with MATLAB toolbox ? 

As far as i can see you are using is designed for wireless communications. My advice is to follow up this into the wireless community: https://community.nxp.com/community/wireless-connectivity 

This community space is for MATLAB related topics.

Thank you!

Daniel

0 Kudos
Reply

1,992 Views
trungosu
Contributor II

I'm using BeyondStudio JN-SW-4141. Thanks

0 Kudos
Reply