Issues with exporting/importing project generated with model based design toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues with exporting/importing project generated with model based design toolbox

1,714件の閲覧回数
fanchang
Contributor I

I had already replace the file to MBD,but it has error.

I"E:\NXP\S32_Power_v1.2/S32DS/e200_ewl2/EWL_C/include" -I"E:\NXP\S32_Power_v1.2/S32DS/e200_ewl2/EWL_C/include/pa" -IF:\PROGRA~2\MATLAB\R2016b\simulink\include\sf_runtime -ID:\matlab\MPC5744\CPconGPIO12_mbd_rtw -ID:\matlab\MPC5744 -ID:\matlab\MPC5744\slx -DUSE_RTMODEL -DMODEL=CPconGPIO12 -DREAL_T=float -DRT -DNUMST=1 -DTID01EQ=0 -DNCSTATES=0 -DMT=0 -DHAVESTDIO
Assembler details : "E:\NXP\S32_Power_v1.2/Cross_Tools/powerpc-eabivle-4_9/bin/powerpc-eabivle-as" -g3 -mbig -mvle -mregnames
Building assembly file crt0.o...
系统找不到指定的路径。
gmake: *** [crt0.o] Error 1

why?how to do?

0 件の賞賛
返信
1 返信

1,582件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi fanchang‌,

Can you please attached your project here to have a look over it.

Thank you!

Daniel

0 件の賞賛
返信