Is MBD Toolbox 1.3.0 Compatible with MATLAB R2024b?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is MBD Toolbox 1.3.0 Compatible with MATLAB R2024b?

Jump to solution
955 Views
Yoshio
Contributor I

When I installed MBD Toolbox 1.3.0 on MATLAB R2024b, most tabs in the Hardware Implementation pane of the configuration parameters were missing, except for Clocking and External Mode.

Is MBD Toolbox 1.3.0 compatible with MATLAB R2024b?

Yoshio_0-1762926415712.png

 

0 Kudos
Reply
1 Solution
934 Views
jack425grace
Contributor I

Hello,

It's almost certain that MBD Toolbox 1.3.0 is not compatible with MATLAB R2024b.

The missing tabs in the Hardware Implementation pane are the classic symptom of an older toolbox failing to recognize or correctly interface with the newer MATLAB/Simulink environment.

View solution in original post

1 Reply
935 Views
jack425grace
Contributor I

Hello,

It's almost certain that MBD Toolbox 1.3.0 is not compatible with MATLAB R2024b.

The missing tabs in the Hardware Implementation pane are the classic symptom of an older toolbox failing to recognize or correctly interface with the newer MATLAB/Simulink environment.