Interrupt-problem with s32k144 devkit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt-problem with s32k144 devkit

ソリューションへジャンプ
3,125件の閲覧回数
lukasschäfer
Contributor III

Hello Community,

i have a problem with the example "FTM Edge Capture" from the Model Based Design Toolbox v2.0 for s32k144.

I connected PTC0 to PTC 15 and measured a PWM.

But the Interrupt service routine is not executed. The LED shines red all the time without blinking.

Thanks for support.

Original Attachment has been moved to: ftm_input_capture_s32k14.mdl.zip

0 件の賞賛
返信
1 解決策
2,911件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi lukasschäfer‌,

If you own a S32K rev1.0 board then please use the Model Based Design Toolbox rev1.0 to program the board.

You can download it from here: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7296847 

Please use the examples from that toolbox.

You should expect this:

1.JPG

2.JPG

Hope this helps!

Daniel

元の投稿で解決策を見る

2 返答(返信)
2,911件の閲覧回数
lukasschäfer
Contributor III

Thank you Daniel.

This is the solution.

Lukas

0 件の賞賛
返信
2,911件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi lukasschäfer‌,

If you own a S32K rev1.0 board then please use the Model Based Design Toolbox rev1.0 to program the board.

You can download it from here: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7296847 

Please use the examples from that toolbox.

You should expect this:

1.JPG

2.JPG

Hope this helps!

Daniel