Hi Im trying to do a SIL implementation with the s32k144 board, Im trying to add a custom code from the hello_world example from s32 Desing Studio. My model in simulink looks likes this...
AlvaroCervantes_0-1711689405162.png
But I dont know in wich block add the code, the code that I am trying to add is the next one...
#define EVB
#ifdef EVB
#define PCC_CLOCK PCC_PORTD_CLOCK
#define LED0_PORT PTD
#define LED0_PIN 15
#define LED1_PORT PTD
#define LED1_PIN 16
#else
#define PCC_CLOCK PCC_PORTC_CLOCK
#define LED0_PORT PTC
#define LED0_PIN 0
#define LED1_PORT PTC
#define LED1_PIN 1
#endif
#include "sdk_project_config.h"
void delay(volatile int cycles)
{
/* Delay function - do nothing for a number of cycles */
while(cycles--);
}
int main(void)
{
status_t error;
/* Configure clocks for PORT */
error = CLOCK_DRV_Init(&clockMan1_InitConfig0);
DEV_ASSERT(error == STATUS_SUCCESS);
/* Set pins as GPIO */
error = PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
DEV_ASSERT(error == STATUS_SUCCESS);
/* Set Output value LED0 & LED1 */
PINS_DRV_SetPins(LED0_PORT, 1 << LED0_PIN);
PINS_DRV_ClearPins(LED1_PORT, 1 << LED1_PIN);
for (;;)
{
/* Insert a small delay to make the blinking visible */
delay(720000);
/* Toggle output value LED0 & LED1 */
PINS_DRV_TogglePins(LED0_PORT, 1 << LED0_PIN);
PINS_DRV_TogglePins(LED1_PORT, 1 << LED1_PIN);
}
}
---end of code
When I click to generate code i got 10 errors, most of them are from undefined variables of the clock.