Including custom code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Including custom code

5,774 Views
raghurajappa
Contributor IV

I am getting an error when I try to build a model which includes custom code. The custom code I used is from https://community.nxp.com/thread/450048  
Please find attached the error. I think it has to do with Simulink 2017b. But I am unable to solve the error. 

0 Kudos
Reply
2 Replies

5,383 Views
mariuslucianand
NXP Employee
NXP Employee

Hello raghurajappa,

Sorry for our delayed answer.

It looks like when compiles, the mwSize variable type has not been defined, probably a file must also be included. 

For this approach of custom code insertion, we also have an example here How to put S32K MCU into sleep (low power mode)? , but just take the .slx model as example, and do not copy those s32k  files into your toolbox because it handles another toolbox. 

Another easier way of injecting custom code into the model is to use the Custom Code blocks from the Simulink Coder (see the image attached), from the Simulink library. The System Initialize block will inject the code in the generated initialize function and the System Outputs blocks will put your code in the step function.

pastedImage_2.png

Hope this helps, 

Marius

0 Kudos
Reply

4,079 Views
AlvaroCervantes
Contributor I

Hi Im trying to do a SIL implementation with the s32k144 board, Im trying to add a custom code from the hello_world example from s32 Desing Studio. My model in simulink looks likes this...

 

AlvaroCervantes_0-1711689405162.pngAlvaroCervantes_0-1711689405162.png

But I dont know in wich block add the code, the code that I am trying to add is the next one...

#define EVB
 
#ifdef EVB
#define PCC_CLOCK PCC_PORTD_CLOCK
#define LED0_PORT PTD
#define LED0_PIN  15
#define LED1_PORT PTD
#define LED1_PIN  16
#else
#define PCC_CLOCK PCC_PORTC_CLOCK
#define LED0_PORT PTC
#define LED0_PIN  0
#define LED1_PORT PTC
#define LED1_PIN  1
#endif
 
#include "sdk_project_config.h"
 
void delay(volatile int cycles)
{
    /* Delay function - do nothing for a number of cycles */
    while(cycles--);
}
 
int main(void)
{
  status_t error;
  /* Configure clocks for PORT */
  error = CLOCK_DRV_Init(&clockMan1_InitConfig0);
  DEV_ASSERT(error == STATUS_SUCCESS);
  /* Set pins as GPIO */
  error = PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
  DEV_ASSERT(error == STATUS_SUCCESS);
 
  /* Set Output value LED0 & LED1 */
  PINS_DRV_SetPins(LED0_PORT, 1 << LED0_PIN);
  PINS_DRV_ClearPins(LED1_PORT, 1 << LED1_PIN);
 
  for (;;)
  {
      /* Insert a small delay to make the blinking visible */
      delay(720000);
 
      /* Toggle output value LED0 & LED1 */
      PINS_DRV_TogglePins(LED0_PORT, 1 << LED0_PIN);
      PINS_DRV_TogglePins(LED1_PORT, 1 << LED1_PIN);
  }
}

 

---end of code

 

When I click to generate code i got 10 errors, most of them are from undefined variables of the clock.

0 Kudos
Reply