How to use MSDI Analog input channels with AMUX and eQADC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use MSDI Analog input channels with AMUX and eQADC?

Jump to solution
2,162 Views
RegulusCheng
Contributor III

Hi, everyone 

I am using RDVCU5775EVM with Simulink 2019b

I had some problems using the analog input channel of MSDI.

I had already tested the digital input channels of MSDI, so the CD1030 chip should work normally. But the user manual of CD1030 didn't say much about the AMUX function, so I don't know if I operate correctly.

I noticed that the User Guide of RDVCU5775EVM mentioned that the main chip uses eQADC channel ANA0 to receive the AMUX input of CD1030, so I just configured the eQADC modules to ANA0 and use it as a normal analog input channel, however, the data I get keep at around 7640(DEC), and no matter what voltage I give it, the data don't change.

I wonder if any other configuration should be done with CD1030 MSDI chips. Please help me.

 

 

 

0 Kudos
Reply
1 Solution
2,142 Views
RegulusCheng
Contributor III

I have solved this problem. Before reading first need to send control instructions to the CD1030 chip through SPI communication to specify the specific pin of AMUX output.
The SPI instruction consists of a 32-bit register, the specific definition of which can be found in the CD1030 datasheet.
After the pin is specified, the analog value can be obtained by reading the ANA0 channel through the eQADC module, with a reading limit of 3.3V. Inputs higher than 3.3V are read as 3.3V.

View solution in original post

0 Kudos
Reply
2 Replies
2,143 Views
RegulusCheng
Contributor III

I have solved this problem. Before reading first need to send control instructions to the CD1030 chip through SPI communication to specify the specific pin of AMUX output.
The SPI instruction consists of a 32-bit register, the specific definition of which can be found in the CD1030 datasheet.
After the pin is specified, the analog value can be obtained by reading the ANA0 channel through the eQADC module, with a reading limit of 3.3V. Inputs higher than 3.3V are read as 3.3V.

0 Kudos
Reply
2,161 Views
RegulusCheng
Contributor III

Here is my model, hope it may help.

0 Kudos
Reply