How to solve License error -1: License missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to solve License error -1: License missing

ソリューションへジャンプ
6,062件の閲覧回数
jordiclos
Contributor I

License Error: -1, Motor Control Toolbox License Missing, please go to The Motor Control Development Toolbox Web Site to purchase a license or request a demo.

I have already install, generate and place the license file (license.lic) into the directory C:\...\MATLAB\MCToolbox\mctbx_Kinetis\lic

Captura.JPG

0 件の賞賛
返信
1 解決策
5,831件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi jordiclos‌,

The "-1" error indicates that the license file can't be found (according with FlexLM error codes: https://community.nxp.com/message/941909?commentID=941909%23comment-941909#comment-908767 )

If you say that you have successfully generated the license for the HostID shown in the picture, and you have save it under the \mctbx_Kinetis\lic\ folder then the only possible scenario that i could think of that may drive you to this failure message is the location of the toolbox.

I see that you have installed it into MATLAB root which is probably under "Program Files". Can you install the toolbox in something like: c:\MCToolbox\mctbx_Kinetis\

Hope it helps!

Daniel

元の投稿で解決策を見る

5 返答(返信)
5,786件の閲覧回数
Gibson_24
Contributor I

I have already install,  place the license file but  some issues accrued so please help me regarding this.

0 件の賞賛
返信
5,779件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @Gibson_24 ,

What toolbox are you using? Make sure you try both with the license extestion .lic and .dat

Regards,

Marius

 

0 件の賞賛
返信
5,773件の閲覧回数
rsating
Contributor III

Be careful how you name the file. It is not enough that the license file extension be correct, the entire filename has to be as expected ("license.dat" or "license.lic") or the activation process will not find the license file. 

5,832件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi jordiclos‌,

The "-1" error indicates that the license file can't be found (according with FlexLM error codes: https://community.nxp.com/message/941909?commentID=941909%23comment-941909#comment-908767 )

If you say that you have successfully generated the license for the HostID shown in the picture, and you have save it under the \mctbx_Kinetis\lic\ folder then the only possible scenario that i could think of that may drive you to this failure message is the location of the toolbox.

I see that you have installed it into MATLAB root which is probably under "Program Files". Can you install the toolbox in something like: c:\MCToolbox\mctbx_Kinetis\

Hope it helps!

Daniel

5,819件の閲覧回数
rsating
Contributor III

It turns out that, not only does the license file have to be in the "lic" subfolder, but it has to be named "license.dat" for "Verify MBD Toolbox License" to find it.  I had bangled "S32K1xx" into the filename, since I have more than one NXP license. That was well intentioned but caused activation to fail. 

It would be nice if the "Activate NXP MBD Toolbox" function re-named the file appropriately as "license.dat" before copying it to the "lic" subfolder for us, or warn us we need to do that. Only after hours of frustration and answers from this thread did I figure out what was wrong.

Thanks

0 件の賞賛
返信