How to debug the MBD generated code in the S32 Design Studio using PEmicro debugger?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to debug the MBD generated code in the S32 Design Studio using PEmicro debugger?

ソリューションへジャンプ
3,021件の閲覧回数
rafael_barbosa
Contributor IV

Hello,

I am using the Devkit MPC5744P and the Model Based Design Toolbox 3.0.0.

I would like to debug the generated code on the target microcontroller using the PEmicro debugger.

What are the steps to import the generated code in the S32 Design Studio in order to run the debugger?

Kind Regards, Rafael

mariuslucianandrei

0 件の賞賛
返信
1 解決策
2,902件の閲覧回数
rafael_barbosa
Contributor IV

Hello mariuslucianandrei

I could use the PEmicro debugger for MBD generated code by importing the project.xml file generated by the MBD toolbox into the S32 Design Studio.

 

pastedImage_1.png

Kind Regards, Rafael

元の投稿で解決策を見る

2 返答(返信)
2,856件の閲覧回数
tl007
Contributor III

Dear @rafael_barbosa 

For some reason, i did the same but was not able to proceed with flashing the new project imported.

Can you maybe provide the next steps?

https://youtu.be/PjFWds2M4nQ

 

0 件の賞賛
返信
2,903件の閲覧回数
rafael_barbosa
Contributor IV

Hello mariuslucianandrei

I could use the PEmicro debugger for MBD generated code by importing the project.xml file generated by the MBD toolbox into the S32 Design Studio.

 

pastedImage_1.png

Kind Regards, Rafael