How to configure this CAN transceiver chip TJA1145A S32K3 MBDT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure this CAN transceiver chip TJA1145A S32K3 MBDT?

1,027 Views
Texhy
Contributor I

How to configure this CAN transceiver chip TJA1145A S32K3 MBDT?Have any engineers configured TJA1145A on MBDT?

0 Kudos
Reply
1 Reply

1,005 Views
SorinIBancila
NXP Employee
NXP Employee

Hello, 

One example of the TJA1145 initialization can be found in the MBD Toolbox for BMS, which you can download and install for free. Please note that the MBD Toolbox for BMS works only with MBD Toolbox for S32K3 version 1.4.0.

 

However, I attached a few imagines of the initialization part for the TJA1145, but also for the SPI configuration. Make sure you follow the schematic for your board, so you initialize the correct SPI instance and properly select the chip select pin. 

SorinIBancila_0-1751467597095.png

SorinIBancila_1-1751467695025.png

SorinIBancila_2-1751467708511.png

 

Best regards,

Sorin Bancila