How does NXP Support Packtage S32K1xx operate without a network

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How does NXP Support Packtage S32K1xx operate without a network

1,796件の閲覧回数
bamboo
Contributor I

S32k_MBD installation package, can only follow the method on the diagram to install it?
You can't just download the package and install it

I hope you can provide the folder of Code in NXP Support Packtage S32K1xx and the subfiles therein.

My personal email: [email protected]

0 件の賞賛
返信
1 返信

1,710件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello bamboo‌,

Obviously you can also download the .mltbx file from here and install it. To not have some issues using the file extension please have a look here MPC57xx..... . Those steps are for MPC but is the same for the S32K.

Best Regards, 

Marius

0 件の賞賛
返信