Getting License error with MBDT Toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting License error with MBDT Toolbox

9,708 Views
harjitsingh
Contributor I

 License Error: -1, Model-Based Design Toolbox License Missing, please go to The Model-Based Design Development Toolbox Web Site to get a free license or request a demo. Provide the following HostID: ec51e3ec

0 Kudos
Reply
7 Replies

8,983 Views
Nikhiladheesh
Contributor II

Hey Marius,

I am facing same issue as mentioned in above thread.

I have actually placed my license.lic files as recommmended by you in exact folders. Still the issue persists.

Help me out here.

Matlab: R2022a

MBDT: MBDToolbox_S32K1xx_4.2.0_20200720.mltbx

Regards,

Nikhil

0 Kudos
Reply

9,596 Views
mariuslucianand
NXP Employee
NXP Employee

Hello harjitsingh‌,

In order to use our MBDT blocks you need to get a free license form the NXP's website using the HostID mentioned in the error message. To do so, please go to https://nxp.flexnetoperations.com/control/frse/product?entitlementId=231620027&lineNum=1&authContact... this page, select the toolbox you need, read our terms and select the License Keys tabs. Press generate and follow the procedure.

pastedImage_1.png

pastedImage_2.png

Once you got the file, please go to the Matlab installation toolbox, find the .src folder, and inside it create a lic folder. In that folder put the generated license. 

Hope this helps,

Marius

0 Kudos
Reply

9,551 Views
orange_
Contributor II

Hello Marius,

 

1.Here is the serial number of my HOST ID;

1.png

 

2.This is my license;

2.png

 

3.This is my MATLAB installation location;

3.png

4.This is where S32K-MBDtoolbox and license are located;

4.png

 

5.This is a mistake that has never been resolved;5.png

 

Please help me! Thanks!

0 Kudos
Reply

9,525 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @orange_ ,

Can you please rename the extension from .dat to .lic?

Hope this helps,

Marius

0 Kudos
Reply

9,495 Views
orange_
Contributor II

Hello Marius,

Thank you for your help.

My problem should appear on the installation path of MATLAB. After modifying the path of MATLAB, the problem has been solved.

Thank you very much for your help!

orange_

9,596 Views
harjitsingh
Contributor I

Hello Marius,

C:\Users\admin\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx

C:\Program Files\MATLAB\R2018b\toolbox

There are the different folder structure. One for the Matlab installation and another where the MBDT is installed.

I am unable to find the .src folder in both the above folder structure.

Following path has .src folder. Kindly advise where to put the license file.

C:\Program Files\MATLAB\R2018b\src

Regards

0 Kudos
Reply

9,596 Views
mariuslucianand
NXP Employee
NXP Employee

Hello harjitsingh‌,

According to your provided path, you have to create a folder "lic" directly in the NXP_MBDToolbox_S32K1xx and inside it to put the license. 

C:\Users\admin\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\lic

Here is a screenshot from my folder path

pastedImage_1.png

Hope this helps,

Marius

0 Kudos
Reply