Freemaster on CAN with other CAN blocks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster on CAN with other CAN blocks

2,667 Views
gmud1234
Contributor II

Is it possible to use Freemaster on CAN, and use the CAN Tx & Rx blocks on the same bus, from within Simulink ?

(our target ECU has no usb/uart interface - just CAN). I am using v4.2 of the MBDT

0 Kudos
Reply
2 Replies

2,621 Views
gmud1234
Contributor II
Thanks for the response.

2,626 Views
SorinIBancila
NXP Employee
NXP Employee

Hello @gmud1234,

Unfortunately, you can't use the same CAN instance for Freemaster and Tx & Rx blocks. If your hardware allows it, you can use one CAN instance for Freemaster and another instance for sending/receiving CAN messages.

Best regards,

Bancila Sorin

0 Kudos
Reply