Fail to use Model-Based Design Toolbox with MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fail to use Model-Based Design Toolbox with MPC5744P

3,820件の閲覧回数
641679783
Contributor II

Hi,

   I,m using the Model-Based Design Toolbox MPC57xx Series, I followed the quick start guide with the uart_hello_world_mpc574xP.mdl example. However, after I click the code generate and build model button in Simulink, and pressed the RESET button, it showed that "Loss communication with CCP MCU. Please cycle power and try again."

   I'm sure that I choose the right COM port and I've successfully flashed some example by S32DS. Also I tried different .rbf files which I found in the community. I heard there are some bugs in S32DS_PA_2.1 with MBDT, shall I try version 2017R1?

   My configuartion is the following:

   S32DS_PA_2.1

   Matlab R2020a

   Model-Based Design Toolbox 3.1.0

   DEVKIT-MPC5744P

S32DS.png

pastedImage_3.png

Best regards!

Kisen

タグ(2)
0 件の賞賛
返信
5 返答(返信)

3,668件の閲覧回数
ranulf
Contributor IV

I have the same problem.

Configuration: 

According to the sticker on the back of the DEVKIT-MPC5744P, The board revision is "SCH-29333 REV E1 700-29333 REV A"

Matlab/Simulink 2020A

Model-Based Design Toolbox MPC57xx Series Version 3.2.0
 

S32 Version 2.1

Windows 10

0 件の賞賛
返信

3,688件の閲覧回数
zzdh
Contributor I

Hello, how do you solve the problem, because I also encountered the same problem?

 

3,682件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @zzdh ,

Which revision of the board are you using?

Regards,

Marius

0 件の賞賛
返信

3,733件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Can you please tell me which revision board are you using?

If you are using the revision E, probably this post might help you https://community.nxp.com/message/1351333?commentID=1351333#comment-1351333 

There serial connected to the OpenSDA differs from one revision to another so the bootloader is different.

Hope this helps,

Marius

0 件の賞賛
返信

3,733件の閲覧回数
641679783
Contributor II

Hello mariuslucianandrei

Thanks for your help.

I'm not sure how to identify the revision, it seems like I'm using a REV B board.

pastedImage_1.png

Also, I've already tried the .rbf file before in https://community.nxp.com/message/1351333?commentID=1351333#comment-1351333, and met the same problem.

0 件の賞賛
返信