FOC Control modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FOC Control modes

2,878件の閲覧回数
mark_chylinski
Contributor I

Hello all!
I'm starting out learning about motor controllers and FOC. I have the S32K144 along with the motor development kit : MTRDEVKSPNK144: S32K144 

I'm struggling quite alot with finding documentation or describtions of the different motor control techniques that are available to the FOC control: in the example code they are in struct "controlStructMode_t" in "motor_structure.h" file. The available modes are Scalar control, voltage control, current control, and speed control. I'd like to know the differences or advantages/disadvantages between them so I can decide on which is best, and why it is better.


I hope someone can point me in the right direction.
Thanks in advance
Mark

3 返答(返信)

2,648件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

I'm not sure what example you are talking about, but I think you can get answers on the S32K community. Here we handle questions regarding MATLAB/Simulink and our toolboxes. We also have materials and examples in our toolboxes that cover motor control topics (e.g. Module 2: PMSM and FOC Theory). If you are interested in this type of development, I could point you to our latest S32K release and you can try it out, but there are some licenses that you'll be needing. Let me know if you want more details about our toolbox and what licenses you'd be needing to run it.

Hope this helps,

Razvan.

2,648件の閲覧回数
mark_chylinski
Contributor I

Hi
Thanks for clearing that up!
I've posted a new question on the S32 community, but the link to the PMSM workshop was very helpful, and indeed some of the control methods are described there, ie. scalar control using V/f, and speed control by implementing a closed speed loop.
I'm still struggling with voltage controlled DQ control and current controlled DQ control setups. But perhaps the other forum will help me out.

Thank you for your time, I appreciate it!
BR
Mark

0 件の賞賛
返信

2,648件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

I'm glat that was helpful. If you are interested we also have a BLDC course (here).

Kind regards,

Razvan.

0 件の賞賛
返信