External Sync for PWM0 (MPC5744P) using MBD not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External Sync for PWM0 (MPC5744P) using MBD not working

5,756 Views
abhishek_kumar1
Contributor IV

Hello All

I tried to use EXT_SYNC for PWM0 module but without success. (for DEVKIT-MPC5744P)

pastedImage_3.png

 

 

For this I created 2 models (for 2 different board, models are attached)

pastedImage_1.jpg

  1.       Syncro_PWM_CTU_External, which sends out a PWM and I use another PWM synchronized with the first one so it acts as EXT_SYNC signal for second board.
  2.       Syncro_PWM_CTU_External_Board2, I used CTU to have PTC15 as an EXT_SYNC Signal. (PTC 15 in DEVKIT was on F:EXRAY module so we removed R27 and used Micro Side Pad and soldered a cable)

 

Somehow the PWM in Syncro_PWM_CTU_External_Board2  (on DEVKIT 2) is not synchronized with Syncro_PWM_CTU_External(on DEVKIT 1)

 

Could you please suggest what is wrong in model “Syncro_PWM_CTU_External_Board2”?

pastedImage_2.png

 mariuslucianandrei‌ [email protected]‌ dumitru-daniel.popa‌

0 Kudos
Reply
11 Replies

5,480 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

So let's summarize a bit your status. As far as I know, you have obtained the sync between PWM0 and PWM1 on a single MPC controller without any external connection and successfully read 4 ADCs at the same time. Am I right?

Now, you need to sync the PWM0 module from one MPC5744P to PWM1 module from another MPC5744P?

Best Regards,

Marius!

0 Kudos
Reply

5,480 Views
abhishek_kumar1
Contributor IV

Dear mariuslucianandrei‌

Let me clarify this.

As far as I know, you have obtained the sync between PWM0 and PWM1 on a single MPC controller without any external connection and successfully read 4 ADCs at the same time. Am I right?

Yes (I have attached a model for this if some one else needs it, 'PWM01_CTU_00_01_ADC0to4.mdl')

Now, you need to sync the PWM0 module from one MPC5744P to PWM1 module from another MPC5744P?

I need to Sync PWM0 (of Board 1) to PWM0 (of Board 2), using EXT_SYNC of PWM0

Hope it is more clear. 

0 Kudos
Reply

5,480 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

From the Reference Manual, I understand that the EXT_SYNC is an input signal. So basically now, you have two inputs connected together, with no signal to trigger them. So the PWM modules would be in sync together but you don't have a signal to sync their reload.

pastedImage_1.png

For PWM block, what the toolbox is not doing right now is to initialize the EXT_Sync pin as input for the PWM. So you need to insert some custom code in order to initialize the pin as EXT_SYNC for PWM. I would also try the following approach: Use the reload interrupt from the PWM0, BRD0 to toggle a pin and use it as input on the PWM0, BRD1.  

pastedImage_2.png

What you could also try is to sync the CTUs from different board since the CTU blocks covers the external in and out pins under the "Pins" tab of the CTU.

Hope this helps,

Marius

0 Kudos
Reply

5,480 Views
abhishek_kumar1
Contributor IV

Dear mariuslucianandrei‌

 

I would also try the following approach: Use the reload interrupt from the PWM0, BRD0 to toggle a pin and use it as input on the PWM0, BRD1.

I do something similar (as explained below)

I have 2 PWM submodules in Model 1 (Board 1), so I use the second PWM submodule only to send a signal (pulse) to Board 2 (ext-sync).

In the end, what I want is that to have the all  PWM of Board 1 in Sync with all PWM of Board 2. (just as we have in one board, i want in both boards and PWM0 allows that using EXT_SYNC)

pastedImage_1.png

What you could also try is to sync the CTUs from different board since the CTU blocks covers the external in and out pins under the "Pins" tab of the CTU.

I have done that in the model (Syncro_PWM_CTU_External_Board2)

pastedImage_4.png

Best Regards

Abhishek

0 Kudos
Reply

5,480 Views
mariuslucianand
NXP Employee
NXP Employee

Hey [email protected]‌,

Regarding what you tried, to sync the modules, as I explained before, the EXT_SYNC pin from the Board 2 should be configured to be input for the PWM0 module. The MBDT now is not doing that initialization, so you need to insert some custom code in order to set PC13 as EXT_SYnc for FLexPWM_0 like in the screenshot added in my last reply. 

Hope this helps, 

Marius

0 Kudos
Reply

5,480 Views
abhishek_kumar1
Contributor IV

Dear mariuslucianandrei‌

I am not able to find the SDK function call (to do INIT_SEL = 3, as in snapshot below), in S32 Design Studio.

Can you help me with this? 

I tried searching INIT_SEL in search but can not find it. 

FlexPWM0.SUB[0].CTRL2.B.INIT_SEL = 3;                   

pastedImage_3.png

0 Kudos
Reply

5,480 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

The init_sel is performed by the pwm block, but the actual pin must be muxed to provide the actual pin signal to the pwm peripheral by writing in the Imcr[87] register and so on.

pastedImage_2.png

Hope this helps, 

Marius

0 Kudos
Reply

5,480 Views
abhishek_kumar1
Contributor IV

Dear mariuslucianandrei‌

Thank you for the hint but I am not able to use Write_Register block.

Also, I did not find IMCR registers here.

I think I am totally misunderstanding, what you are asking me to do. 

We have already said in the Simulink block that it is an external Sync

The only thing needed to be done is to define the PIN for the EXT_SYNC.

I am very lost now. 

pastedImage_1.png

Best Regards,

Abhishek 

0 Kudos
Reply

5,480 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

We will investigate the error regarding the register. 

However, in order to initialize the external pin to redirect the signal to the PWM0 you need to insert a custom code, declaring the structure attached tin the text file pwmSyncPinsCfg and then call the  two functions below the structure declaration. 

If you need an example on how to insert the custom code, in our toolbox you will find a model called "custom_code.mdl". Consider adding the code from the attached file in the System Initialize block like in the model.

pastedImage_1.png

Hope this helps you,

Marius

0 Kudos
Reply

5,479 Views
abhishek_kumar1
Contributor IV

Dear mariuslucianandrei‌

Thank you for the hint.

I tried to do the changes

1. Added the code you sent in Syncro_PWM_CTU_External_Board2.mdl

2. Removed the CTU block from "Syncro_PWM_CTU_External_Board2.mdl"

Still the synchronization could not be achieved. 

I have attached the model which is in Board 1 (which sends a signal to reset PWM timer for board 2)

Please provide the your input.

Best Regards

Abhishek

0 Kudos
Reply

5,480 Views
abhishek_kumar1
Contributor IV

Dear mariuslucianandrei‌

It has been some time, but have you found any solution regrading External PWM Sync. We are planning to use this feature but were not able to work it out yet. 

Let us know of any solution.

Best Regards, 

Abhishek 

[email protected]‌ 

0 Kudos
Reply