Error reported by S-function, validity of the Simulink block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error reported by S-function, validity of the Simulink block

1,129 Views
RobSpanjers
NXP Employee
NXP Employee

Hello,

When building a Motor Control for the S32K344 in Simulink, I get the following error:

"Error reported by S-function 'GFLIB_SinCos_SF_FLT' in 's32k344_MC_Test_ebt/FastLoopControl/GFLIB_SinCos_FLT/GFLIB_SinCos_SF': Unexpected error when checking the validity of the Simulink Bus/StructType 'SWLIBS_2Syst_FLT'"

It says it is a Block diagram error of the standard AMMCLIB_s32k3xx blocks used.

RobSpanjers_0-1668587808764.png

I have the toolbox on my laptop and also added in the folder of the project I'm working on, but it doesn't work.

 

How to solve this error?

 

Kind regards,

Rob Spanjers

 

0 Kudos
Reply
0 Replies