Error Pil example MBDT S12ZVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error Pil example MBDT S12ZVM

1,474件の閲覧回数
Stefan_9811
Contributor II

Dear all,

 

we installed the Model Based Design Toolbox (MBDT) for S12zvm and tried to run the provided example for the PIL Simulation. Unfortunately we get an error when we try to start the Simulation. 

The steps we take are:

  1. Open model "sim_pil_test_s12zvm"
  2. Select our target and enable pil simulation in the configuration Block
  3. Select Subsystem=>Tools=>NXP Model-Based Design Toolbox for S12zvm => To Pil Mode on Mc9S12ZVM

Unfortunately we still get the attached error. 

We are using the #MC9S12ZVM High current Board with Matlab 2019b and the MinGW64 mex compiler.

Has anyone a suggestion? 

Kind regards.

@paulvlase @Daniel_Popa 

0 件の賞賛
返信
1 返信

1,364件の閲覧回数
paulvlase
NXP Employee
NXP Employee

Hello @Stefan_9811 ,

 

Can you try to apply the attached patch MBDToolbox_S12ZVMx_1.4.0_patch_03072023.exe.zip and run PIL simulation again?

 

Steps to apply the patch:

1. Download the attached zip file and unzip it.

2. Open Matlab and run mbd_find_s12z_root() to get the root folder there the S12ZVM toolbox is installed.

3. Close Matlab.

4. Open the MBDToolbox_S12ZVMx_1.4.0_patch_03072023.exe.zip file and extract it's contents to the root folder of the toolbox.

 

Regards,

Paul

0 件の賞賛
返信