Encoder for HVP-MC3PH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encoder for HVP-MC3PH

1,874件の閲覧回数
lethuer
Contributor V

Hi,

the HVP-MC3PH: High-Voltage Development Platform supports a motor speed/position sensors interface (Encoder, Hall, Tacho Generator)

In the circuit diagram I saw a 5 pin connector (J9) for the encoder Interface with a 5V power supply.Encoder Interface.PNG

Is there a recommendation for a Encoder working together with the platform ?

Best regards

0 件の賞賛
返信
2 返答(返信)

1,688件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi lethuer2‌,

Any quadrature encoder that works at 5V should be fine. Since the board supplies 5V as available power for the encoder, it is expecting a 5V signal as the output from the encoder. If this is not the case for your encoder, additional circuitry to translate the voltage level might be required.

Nevertheless, I'm not aware of any recommendation. Please check this manual to see how an encoder can be used: 

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/DRM105.pdf 

Hope it helps!

Daniel

0 件の賞賛
返信

1,688件の閲覧回数
lethuer
Contributor V

Okay, so for example this one should be fine ?

Encoder.jpg

https://www.conrad.de/de/drehgeber-1-st-iduino-se055-1485328.html

0 件の賞賛
返信